BasePartTransientStatus_Struct Struct¶
NXOpen.BasePart.TransientStatus is an alias for NXOpen.BasePartTransientStatus_Struct
-
class
NXOpen.
BasePartTransientStatus_Struct
¶ Bases:
object
Transient part return data
Fields¶
Field | Description |
---|---|
Trans | Part is transient |
InitiallyTransient | Did part start out in a transient state |
Locked | Part is locked in a transient state |
TransientChildren | Part has transient children |
Trans¶
-
BasePartTransientStatus_Struct.
Trans
¶ Part is transient
-------------------------------------
Getter Method Signature
Trans()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
Trans(value)
Parameters: value (bool) –
InitiallyTransient¶
-
BasePartTransientStatus_Struct.
InitiallyTransient
¶ Did part start out in a transient state
-------------------------------------
Getter Method Signature
InitiallyTransient()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
InitiallyTransient(value)
Parameters: value (bool) –
Locked¶
-
BasePartTransientStatus_Struct.
Locked
¶ Part is locked in a transient state
-------------------------------------
Getter Method Signature
Locked()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
Locked(value)
Parameters: value (bool) –
TransientChildren¶
-
BasePartTransientStatus_Struct.
TransientChildren
¶ Part has transient children
-------------------------------------
Getter Method Signature
TransientChildren()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
TransientChildren(value)
Parameters: value (bool) –