ProductOutlineManager Class¶
-
class
NXOpen.Assemblies.
ProductOutlineManager
¶ Bases:
object
Represents a collection of assemblies
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
IsProductOutlineDefined | Returns the status of the product outline. |
Methods¶
Method | Description |
---|---|
CreateProductOutlineBuilder | Creates a NXOpen.Assemblies.ProductOutlineBuilder . |
ShowProductOutline | Controls the visibility of already defined product outline. |
ShowSelectableProductOutline | Controls the visibility and selectability of already defined product outline. |
Property Detail¶
IsProductOutlineDefined¶
-
ProductOutlineManager.
IsProductOutlineDefined
¶ Returns the status of the product outline.
If the product outline is already defined, it returns “true”, else returns “false”.
-------------------------------------
Getter Method
Signature
IsProductOutlineDefined()
Returns: Return value for the status of the product outline. Return type: bool New in version NX6.0.0.
License requirements: None.
Method Detail¶
CreateProductOutlineBuilder¶
-
ProductOutlineManager.
CreateProductOutlineBuilder
¶ Creates a
NXOpen.Assemblies.ProductOutlineBuilder
.Gives access to the attributes of the Product Outline
Signature
CreateProductOutlineBuilder()
Returns: Return type: NXOpen.Assemblies.ProductOutlineBuilder
New in version NX6.0.0.
License requirements: adv_assemblies (“ADVANCED ASSEMBLIES”)
ShowProductOutline¶
-
ProductOutlineManager.
ShowProductOutline
¶ Controls the visibility of already defined product outline.
Supply **true</b> to show the Product Outline, or **false</b> to hide the Product Outline.
Signature
ShowProductOutline(isShow)
Parameters: isShow (bool) – Flag to make the product Outline selectable or unselectable. If “true” the Product outline is made selectable. New in version NX6.0.0.
License requirements: adv_assemblies (“ADVANCED ASSEMBLIES”)
ShowSelectableProductOutline¶
-
ProductOutlineManager.
ShowSelectableProductOutline
¶ Controls the visibility and selectability of already defined product outline.
Supply **true</b> to show the selectable Product Outline, or **false</b> to hide the Product Outline.
Signature
ShowSelectableProductOutline(isSelectable)
Parameters: isSelectable (bool) – Flag to make the product Outline selectable or unselectable. If “true” the Product outline is made selectable. New in version NX6.0.0.
License requirements: adv_assemblies (“ADVANCED ASSEMBLIES”)