PositionOverrideType Enumeration¶
-
class
NXOpen.Assemblies.
PositionOverrideType
¶ Bases:
object
Represents the type of the positioning override on the component Enum Members
Enum Member Enum Member Description None No position overrideUnloaded Position overridden, but in an unloaded parentExplicit Position explicitly overridden by userMatingImplicit Position implicitly overridden because of mating conditionsConstraintImplicit Position implicitly overridden because of assembly constraints-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-