MakeUniquePartBuilder Class¶
-
class
NXOpen.Assemblies.
MakeUniquePartBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Assemblies.MakeUniquePartBuilder
builderTo create a new instance of this class, use
NXOpen.Assemblies.AssemblyManager.CreateMakeUniquePartBuilder
Default values.
Property Value CopyChoices CopyAssemblyOnly New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
CopyChoices | Returns or sets the copy choices returned. |
SelectedComponents | Returns the selected components to be made unique are returned. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MakeUniquePartBuilderOption Enumeration | Represents possible copy assembly options for unique part |
Property Detail¶
CopyChoices¶
-
MakeUniquePartBuilder.
CopyChoices
¶ Returns or sets the copy choices returned.
-------------------------------------
Getter Method
Signature
CopyChoices()
Returns: Return type: NXOpen.Assemblies.MakeUniquePartBuilderOption
New in version NX8.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
-------------------------------------
Setter Method
Signature
CopyChoices(copyChoices)
Parameters: copyChoices ( NXOpen.Assemblies.MakeUniquePartBuilderOption
) –New in version NX8.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
SelectedComponents¶
-
MakeUniquePartBuilder.
SelectedComponents
¶ Returns the selected components to be made unique are returned.
-------------------------------------
Getter Method
Signature
SelectedComponents()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX8.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
Method Detail¶
Validate¶
-
MakeUniquePartBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.