ComponentPattern Class¶
-
class
NXOpen.Assemblies.
ComponentPattern
¶ Bases:
NXOpen.NXObject
Represents the component pattern class.
To create or edit an instance of this class, use
NXOpen.Assemblies.ComponentPatternBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
ChangeReferencePatternTemplate | Changes the template component of a reference pattern to a pattern member at indices (firstBaseInstanceIndex, secondBaseInstanceIndex). |
Delete | Deletes the component pattern object. |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
DisplayInformation | Displays the information of the component pattern. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAllPatternMembers | Returns all the pattern members. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComponentsToPattern | Gets all the Assemblies.Component that are selected for component pattern. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetPatternDeferredStatus | Gets the deferred status of the component pattern. |
GetPatternName | Gets the component pattern name. |
GetPatternSuppressedStatus | Gets the suppressed status of the component pattern. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
LoadRelatedGeometry | Loads the parts containing data referenced by this pattern, including the parts that are patterned and parts containing the objects that define the pattern parameters. |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Suppress | Suppresses the component pattern object. |
Unsuppress | Unsuppresses the component pattern object. |
Property Detail¶
IsOccurrence¶
-
ComponentPattern.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
ComponentPattern.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
ComponentPattern.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
ComponentPattern.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
ComponentPattern.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
ComponentPattern.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
ChangeReferencePatternTemplate¶
-
ComponentPattern.
ChangeReferencePatternTemplate
¶ Changes the template component of a reference pattern to a pattern member at indices (firstBaseInstanceIndex, secondBaseInstanceIndex).
Signature
ChangeReferencePatternTemplate(firstBaseInstanceIndex, secondBaseInstanceIndex)
Parameters: - firstBaseInstanceIndex (int) –
- secondBaseInstanceIndex (int) –
New in version NX9.0.0.
License requirements: None.
Delete¶
-
ComponentPattern.
Delete
¶ Deletes the component pattern object.
Signature
Delete(deleteComponents)
Parameters: deleteComponents (bool) – New in version NX9.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
DisplayInformation¶
-
ComponentPattern.
DisplayInformation
¶ Displays the information of the component pattern.
Signature
DisplayInformation()
New in version NX9.0.0.
License requirements: None.
FindObject¶
-
ComponentPattern.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetAllPatternMembers¶
-
ComponentPattern.
GetAllPatternMembers
¶ Returns all the pattern members.
Signature
GetAllPatternMembers()
Returns: Return type: list of NXOpen.Assemblies.PatternMember
New in version NX9.0.0.
License requirements: None.
GetComponentsToPattern¶
-
ComponentPattern.
GetComponentsToPattern
¶ Gets all the
Assemblies.Component
that are selected for component pattern.Signature
GetComponentsToPattern()
Returns: Return type: list of NXOpen.Assemblies.Component
New in version NX9.0.0.
License requirements: None.
GetPatternDeferredStatus¶
-
ComponentPattern.
GetPatternDeferredStatus
¶ Gets the deferred status of the component pattern.
Signature
GetPatternDeferredStatus()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
GetPatternName¶
-
ComponentPattern.
GetPatternName
¶ Gets the component pattern name.
Signature
GetPatternName()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
GetPatternSuppressedStatus¶
-
ComponentPattern.
GetPatternSuppressedStatus
¶ Gets the suppressed status of the component pattern.
Signature
GetPatternSuppressedStatus()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
Print¶
-
ComponentPattern.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
ComponentPattern.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.