ArrangementCollection Class¶
-
class
NXOpen.Assemblies.
ArrangementCollection
¶ Bases:
object
a collection of arrangements
To obtain an instance of this class, refer to
NXOpen.Assemblies.ComponentAssembly
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
Create | Creates a standard NXOpen.Assemblies.Arrangement , based on an existing standard NXOpen.Assemblies.Arrangement . |
CreateIsolated | Creates an isolated NXOpen.Assemblies.Arrangement , based on an existing NXOpen.Assemblies.Arrangement NXOpen.Assemblies.Arrangement . |
FindObject | Finds the NXOpen.Assemblies.Arrangement with the given identifier as recorded in a journal. |
Method Detail¶
Create¶
-
ArrangementCollection.
Create
¶ Creates a standard
NXOpen.Assemblies.Arrangement
, based on an existing standardNXOpen.Assemblies.Arrangement
.Note that any
NXOpen.Assemblies.ComponentAssembly
that contains components will have at least one standardNXOpen.Assemblies.Arrangement
.See
Assemblies.ComponentAssembly.ActiveArrangement
.Note that the existing
NXOpen.Assemblies.Arrangement
must not be isolated.Signature
Create(templateArrangement, name)
Parameters: - templateArrangement (
NXOpen.Assemblies.Arrangement
) – The originalNXOpen.Assemblies.Arrangement
. The newNXOpen.Assemblies.Arrangement
will be copied from this. ThisNXOpen.Assemblies.Arrangement
must not be isolated. - name (str) – The name of the new arrangement NOTE: The full Unicode character set is not supported for this parameter.
Returns: The new arrangement
Return type: New in version NX3.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
- templateArrangement (
CreateIsolated¶
-
ArrangementCollection.
CreateIsolated
¶ Creates an isolated
NXOpen.Assemblies.Arrangement
, based on an existingNXOpen.Assemblies.Arrangement
NXOpen.Assemblies.Arrangement
.Note that any
NXOpen.Assemblies.ComponentAssembly
that contains components will have at least one standardNXOpen.Assemblies.Arrangement
.See
Assemblies.ComponentAssembly.ActiveArrangement
.Note that the existing
NXOpen.Assemblies.Arrangement
must not be isolated.Signature
CreateIsolated(templateArrangement, name)
Parameters: - templateArrangement (
NXOpen.Assemblies.Arrangement
) – The originalNXOpen.Assemblies.Arrangement
. ThisNXOpen.Assemblies.Arrangement
must not be isolated. - name (str) – The name of the new
NXOpen.Assemblies.Arrangement
. NOTE: The full Unicode character set is not supported for this parameter.
Returns: The new
NXOpen.Assemblies.Arrangement
.Return type: New in version NX9.0.1.
License requirements: assemblies (“ASSEMBLIES MODULE”)
- templateArrangement (
FindObject¶
-
ArrangementCollection.
FindObject
¶ Finds the
NXOpen.Assemblies.Arrangement
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Name of the arrangement to be found Returns: Arrangement found, or null if no such arrangement exists. Return type: NXOpen.Assemblies.Arrangement
New in version NX3.0.0.
License requirements: None.