SymbolPreferencesOption Enumeration¶
-
class
NXOpen.Annotations.
SymbolPreferencesOption
¶ Bases:
object
Specifies the custom symbol preferences for the following -
Crosshatch
Area fill
Color, font and line width
This option is only available when creating. Enum Members
Enum Member Enum Member Description PartSymbol Specifies part’s symbol preferences will be usedMasterSymbol Specifies master symbol’s preferences will be usedLast Last enum value. Should not be used.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-