SymbolFileCollection Class¶
-
class
NXOpen.Annotations.
SymbolFileCollection
¶ Bases:
object
Represents a collection of
NXOpen.Annotations.SymbolFile
objectsUse
NXOpen.Annotations.SymbolFile
to get the instance of this class.New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
CreateSymbolFileBuilder | Creates a drafting symbol file builder @return |
FindObject | Finds the NXOpen.Annotations.SymbolFile with the given name. |
Method Detail¶
CreateSymbolFileBuilder¶
-
SymbolFileCollection.
CreateSymbolFileBuilder
¶ Creates a drafting symbol file builder
Signature
CreateSymbolFileBuilder(object)
Parameters: object ( NXOpen.Annotations.SymbolFile
) –Returns: Return type: NXOpen.Annotations.SymbolFileBuilder
New in version NX8.0.0.
License requirements: nx_layout (“NX Layout”)
FindObject¶
-
SymbolFileCollection.
FindObject
¶ Finds the
NXOpen.Annotations.SymbolFile
with the given name.An exception will be thrown if no object can be found with the given name.
Signature
FindObject(name)
Parameters: name (str) – Region name:Associated object index Returns: Symbol file object Return type: NXOpen.Annotations.SymbolFile
New in version NX8.0.0.
License requirements: None.