SurfaceFinishBuilderStandardType Enumeration¶
NXOpen.Annotations.SurfaceFinishBuilder.StandardType is an alias for NXOpen.Annotations.SurfaceFinishBuilderStandardType
-
class
NXOpen.Annotations.
SurfaceFinishBuilderStandardType
¶ Bases:
object
the valid types for pmi surface finish standards
Enum Members
Enum Member Enum Member Description Ansi ANSIIso ISOJis JISDin DINIso2002 ISO 2002Din2002 DIN 2002Gb GB131-93Eskd ESKD-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-