SurfaceFinishBuilderFinishType Enumeration¶
NXOpen.Annotations.SurfaceFinishBuilder.FinishType is an alias for NXOpen.Annotations.SurfaceFinishBuilderFinishType
-
class
NXOpen.Annotations.
SurfaceFinishBuilderFinishType
¶ Bases:
object
the valid types for pmi finish type
Enum Members
Enum Member Enum Member Description Basic BasicModifier ModifierModifierAllAround Modifier, All AroundMaterialRemovalRequired Material Removal RequiredModifierMaterialRemovalRequired Modifier, Material Removal RequiredModifierMaterialRemovalRequiredAllAround Modifier, Material Removal Required, All AroundMaterialRemovalProhibited Material Removal ProhibitedModifierMaterialRemovalProhibited Modifier, Material Removal ProhibitedModifierMaterialRemovalProhibitedAllAround Modifier, Material Removal Prohibited, All Around-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-