SearchCriteriaSurfaceFinishBuilderSurfaceFinishTypes Enumeration¶
NXOpen.Annotations.SearchCriteriaSurfaceFinishBuilder.SurfaceFinishTypes is an alias for NXOpen.Annotations.SearchCriteriaSurfaceFinishBuilderSurfaceFinishTypes
-
class
NXOpen.Annotations.
SearchCriteriaSurfaceFinishBuilderSurfaceFinishTypes
¶ Bases:
object
Lists the search pmi surface finish type
Enum Members
Enum Member Enum Member Description Open openOpenAndModifier open and modifierOpenAndModifierAndAllAround opem and modifier and all aroundRequired requiredRequiredAndModifier required and modifierRequiredAndModifierAndAllAround required and modifier and all aroundProhibited prohibitedProhibitedAndModifier prohibiter and modifierProhibitedAndModifierAndAllAround prohibiter and modifier and all around-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-