SearchCriteriaFeatureControlFrameBuilderPrimaryDatumMCMOptions Enumeration¶
NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilder.PrimaryDatumMCMOptions is an alias for NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderPrimaryDatumMCMOptions
-
class
NXOpen.Annotations.
SearchCriteriaFeatureControlFrameBuilderPrimaryDatumMCMOptions
¶ Bases:
object
Lists the type of pmi feature control frame primary datum MCM
Enum Members
Enum Member Enum Member Description None noneLeastMaterialCondition least material conditionMaximumMaterialCondition maximum material conditionRegardlessofFeatureSize regardless of feature size-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-