PmiOrdinateDimensionBuilder Class¶
-
class
NXOpen.Annotations.
PmiOrdinateDimensionBuilder
¶ Bases:
NXOpen.Annotations.BaseOrdinateDimensionBuilder
Represents a
Annotations.OrdinateDimension
builderTo create a new instance of this class, use
NXOpen.Annotations.DimensionCollection.CreatePmiOrdinateDimensionBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ActiveHorizontalMargin | Returns or sets the active horizontal margin(defined or inferred) where horizontal dimension will be automatically placed. |
ActiveVerticalMargin | Returns or sets the active vertical margin(defined or inferred) where horizontal dimension will be automatically placed. |
AllowDuplicates | Returns or sets the allow duplicates |
AppendedText | Returns the appended text |
AssociatedObjects | Returns the associated objects |
AutoAssociativities | Returns the auto ordinate associativities |
Baseline | Returns the baseline |
HorizontalInferredMarginLocation | Returns or sets the horizontal inferred margin location |
Inherit | Returns the inherit |
OrdinateOrigin | Returns the ordinate origin |
Origin | Returns the origin |
RespositionExisting | Returns or sets the resposition existing |
SecondAssociativities | Returns the second associativities |
Style | Returns the style |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type |
VerticalInferredMarginLocation | Returns or sets the vertical inferred margin location |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AssociatedObjects¶
-
PmiOrdinateDimensionBuilder.
AssociatedObjects
¶ Returns the associated objects
-------------------------------------
Getter Method
Signature
AssociatedObjects()
Returns: Return type: NXOpen.Annotations.AssociatedObjectsBuilder
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
PmiOrdinateDimensionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.