OrdinatePositiveDirection Enumeration¶
-
class
NXOpen.Annotations.
OrdinatePositiveDirection
¶ Bases:
object
Specifies the positive direction for ordinate dimensions Enum Members
Enum Member Enum Member Description All Specifies positive direction for all dimensionsUpperRight Specifies positive direction for dimensions in upper right qudrantUpperLeft Specifies positive direction for dimensions in upper left qudrantLowerRight Specifies positive direction for dimensions in lower right qudrantLowerLeft Specifies positive direction for dimensions in lower left qudrantLast Last enum value. Should not be used.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-