OrdinateMarginCollection Class¶
-
class
NXOpen.Annotations.
OrdinateMarginCollection
¶ Bases:
object
Represents a collection of
NXOpen.Annotations.OrdinateMargin
To obtain an instance of this class, refer to
NXOpen.Annotations.AnnotationManager
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
AddMargin | Adds an ordinate margin object @return |
CreateHorizontalMargin | Creates a horizontal ordinate margin object @return New horizontal ordinate margin |
CreateInferredMargin | Creates an inferred ordinate margin object @return |
CreateVerticalMargin | Creates a vertical ordinate margin object @return New vertical ordinate margin |
Method Detail¶
AddMargin¶
-
OrdinateMarginCollection.
AddMargin
¶ Adds an ordinate margin object
Signature
AddMargin(ordinateOrigin, editMargin, offsetDistance)
Parameters: - ordinateOrigin (
NXOpen.Annotations.OrdinateOriginDimension
) – Ordinate origin dimension - editMargin (
NXOpen.Annotations.OrdinateMargin
) – existing margin - offsetDistance (float) – Margin offset distance
Returns: Return type: New in version NX5.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
- ordinateOrigin (
CreateHorizontalMargin¶
-
OrdinateMarginCollection.
CreateHorizontalMargin
¶ Creates a horizontal ordinate margin object
Signature
CreateHorizontalMargin(ordinateOrigin, associativity, offsetDistance)
Parameters: - ordinateOrigin (
NXOpen.Annotations.OrdinateOriginDimension
) – Ordinate origin dimension - associativity (
NXOpen.Annotations.Associativity
) – Associativity data for the ordinate margin - offsetDistance (float) – Margin offset distance
Returns: New horizontal ordinate margin
Return type: New in version NX4.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
- ordinateOrigin (
CreateInferredMargin¶
-
OrdinateMarginCollection.
CreateInferredMargin
¶ Creates an inferred ordinate margin object
Signature
CreateInferredMargin(ordinateOrigin, origin, subtype)
Parameters: - ordinateOrigin (
NXOpen.Annotations.OrdinateOriginDimension
) – Ordinate origin dimension - origin (
NXOpen.Point3d
) – Margin point in dimension entity space - subtype (int) – Ordinate margin subtype
Returns: Return type: New in version NX5.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
- ordinateOrigin (
CreateVerticalMargin¶
-
OrdinateMarginCollection.
CreateVerticalMargin
¶ Creates a vertical ordinate margin object
Signature
CreateVerticalMargin(ordinateOrigin, associativity, offsetDistance)
Parameters: - ordinateOrigin (
NXOpen.Annotations.OrdinateOriginDimension
) – Ordinate origin dimension - associativity (
NXOpen.Annotations.Associativity
) – Associativity data for the ordinate margin - offsetDistance (float) – Margin offset distance
Returns: New vertical ordinate margin
Return type: New in version NX4.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
- ordinateOrigin (