OrdinateDoglegDefinition Enumeration¶
-
class
NXOpen.Annotations.
OrdinateDoglegDefinition
¶ Bases:
object
Specifies the ordinate dimension dogleg definition
A - Start offset
B - End offset
C - Dog leg angle
<code> _____________ Dimension Line | | B | _______ | A / / . / .C / Dogleg Segement . / _______./ | | </code>
Enum Members
Enum Member Enum Member Description StartAndEnd Specifies start and end offeset definedStartAngle Specifies start offset and dogleg angle definedEndAngle Specifies end offset and dogleg angle definedLast Last enum value. Should not be used.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-