OrdinateDoglegCreationOption Enumeration¶
-
class
NXOpen.Annotations.
OrdinateDoglegCreationOption
¶ Bases:
object
Specifies the dogleg creation option when creating/editing the ordinate dimension Enum Members
Enum Member Enum Member Description Infer Software infers whether the dogleg would be createdYes Dogleg will always be createdNo Dogleg will not be createdLast Last enum value. Should not be used.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-