OrdinateBaselineBuilder Class¶
-
class
NXOpen.Annotations.
OrdinateBaselineBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a builder for an ordinate baseline
This is a sub-builder class and cannot be directly instantiated
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ActivateBaseline | Returns or sets the activate baseline |
ActivatePerpendicular | Returns or sets the activate perpendicular |
BaselineVector | Returns or sets the baseline vector |
IsBaselineDirectionReversed | Returns or sets a flag indicating if the positive measurement direction for the baseline is reversed |
IsPerpendicularBaselineDirectionReversed | Returns or sets a flag indicating if the positive measurement direction for the perpendicular baseline is reversed |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ActivateBaseline¶
-
OrdinateBaselineBuilder.
ActivateBaseline
¶ Returns or sets the activate baseline
-------------------------------------
Getter Method
Signature
ActivateBaseline()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActivateBaseline(active)
Parameters: active (bool) – New in version NX9.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
ActivatePerpendicular¶
-
OrdinateBaselineBuilder.
ActivatePerpendicular
¶ Returns or sets the activate perpendicular
-------------------------------------
Getter Method
Signature
ActivatePerpendicular()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActivatePerpendicular(active)
Parameters: active (bool) – New in version NX9.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
BaselineVector¶
-
OrdinateBaselineBuilder.
BaselineVector
¶ Returns or sets the baseline vector
-------------------------------------
Getter Method
Signature
BaselineVector()
Returns: Return type: NXOpen.Direction
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BaselineVector(baselineVector)
Parameters: baselineVector ( NXOpen.Direction
) –New in version NX9.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
IsBaselineDirectionReversed¶
-
OrdinateBaselineBuilder.
IsBaselineDirectionReversed
¶ Returns or sets a flag indicating if the positive measurement direction for the baseline is reversed
-------------------------------------
Getter Method
Signature
IsBaselineDirectionReversed()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsBaselineDirectionReversed(isReversed)
Parameters: isReversed (bool) – New in version NX9.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
IsPerpendicularBaselineDirectionReversed¶
-
OrdinateBaselineBuilder.
IsPerpendicularBaselineDirectionReversed
¶ Returns or sets a flag indicating if the positive measurement direction for the perpendicular baseline is reversed
-------------------------------------
Getter Method
Signature
IsPerpendicularBaselineDirectionReversed()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsPerpendicularBaselineDirectionReversed(isReversed)
Parameters: isReversed (bool) – New in version NX9.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
OrdinateBaselineBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.