OffsetCenterPointCollection Class¶
-
class
NXOpen.Annotations.
OffsetCenterPointCollection
¶ Bases:
object
Represents a collection of
NXOpen.Annotations.OffsetCenterPoint
objectsTo obtain an instance of this class, refer to
NXOpen.Annotations.AnnotationManager
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreateOffsetCenterPointBuilder | Creates the OffsetCenterPointBuilder @return OffsetCenterPointCenterlineBuilder object |
FindObject | Finds the offset center point with the given name. |
Method Detail¶
CreateOffsetCenterPointBuilder¶
-
OffsetCenterPointCollection.
CreateOffsetCenterPointBuilder
¶ Creates the OffsetCenterPointBuilder
Signature
CreateOffsetCenterPointBuilder(centerPoint)
Parameters: centerPoint ( NXOpen.Annotations.OffsetCenterPoint
) –NXOpen.Annotations.OffsetCenterPoint
to be edited, if None then create a new oneReturns: OffsetCenterPointCenterlineBuilder object Return type: NXOpen.Annotations.OffsetCenterPointBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
FindObject¶
-
OffsetCenterPointCollection.
FindObject
¶ Finds the offset center point with the given name.
An exception will be thrown if no object can be found with given name
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier of the offset center point to be found Returns: OffsetCenterPoint with this identifier Return type: NXOpen.Annotations.OffsetCenterPoint
New in version NX6.0.0.
License requirements: None.