NarrowDisplayOption Enumeration¶
-
class
NXOpen.Annotations.
NarrowDisplayOption
¶ Bases:
object
Specifies the narrow dimension display option Enum Members
Enum Member Enum Member Description None Doesn’t display narrow dimensionNoLeader Displays narrow dimension without leaderWithLeaderNoStub Displays narrow dimension with leader, but without stubAboveStub Displays narrow dimension above stubAfterStub Displays narrow dimension after stubLast Last enum value. Should not be used.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-