LinearDimensionBuilder Class¶
-
class
NXOpen.Annotations.
LinearDimensionBuilder
¶ Bases:
NXOpen.Annotations.BaseLinearDimensionBuilder
Represents a
Annotations.Dimension
builderTo create a new instance of this class, use
NXOpen.Annotations.DimensionCollection.CreateLinearDimensionBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AppendedText | Returns the appended text |
DimensionSet | Returns the dimension set |
Driving | Returns the driving |
FirstAssociativity | Returns the first associativity. |
ForeshorteningSymbol | Returns the foreshortening symbol builder |
Inherit | Returns the inherit |
Measurement | Returns the measurement |
MeasurementType | Returns or sets the measurement type |
Origin | Returns the origin |
SecondAssociativity | Returns the second associativity. |
Style | Returns the style |
Tag | Returns the Tag for this object. |
UseBaseline | Returns or sets a treat first associativity as a baseline |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Driving¶
-
LinearDimensionBuilder.
Driving
¶ Returns the driving
-------------------------------------
Getter Method
Signature
Driving()
Returns: Return type: NXOpen.Annotations.DrivingValueBuilder
New in version NX9.0.0.
License requirements: None.
ForeshorteningSymbol¶
-
LinearDimensionBuilder.
ForeshorteningSymbol
¶ Returns the foreshortening symbol builder
-------------------------------------
Getter Method
Signature
ForeshorteningSymbol()
Returns: Return type: NXOpen.Annotations.ForeshorteningSymbolBuilder
New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
LinearDimensionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.