LineWeldSideData Class¶
-
class
NXOpen.Annotations.
LineWeldSideData
¶ Bases:
NXOpen.TransientObject
Represents line weld side data
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
DepthRootOpeningNumberOfWelds | Returns or sets the depth or root opening or number of welds as the case may be |
FinishMethod | Returns or sets the weld finish method |
GrooveAngle | Returns or sets the groove angle |
LengthPitch | Returns or sets the weld length and pitch |
Size | Returns or sets the weld size |
SizeLetterCode | Returns or sets the weld size letter code (ISO and DIN only) |
SupplementarySymbol | Returns or sets the weld supplementary symbol |
Symbol | Returns or sets the elementary weld symbol |
Property Detail¶
DepthRootOpeningNumberOfWelds¶
-
LineWeldSideData.
DepthRootOpeningNumberOfWelds
¶ Returns or sets the depth or root opening or number of welds as the case may be
-------------------------------------
Getter Method
Signature
DepthRootOpeningNumberOfWelds()
Returns: Depth or root opening or number of welds Return type: str New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DepthRootOpeningNumberOfWelds(depthRootOpeningNumWeld)
Parameters: depthRootOpeningNumWeld (str) – New depth or root opening or number of welds New in version NX4.0.0.
License requirements: None.
FinishMethod¶
-
LineWeldSideData.
FinishMethod
¶ Returns or sets the weld finish method
-------------------------------------
Getter Method
Signature
FinishMethod()
Returns: Finish method Return type: NXOpen.Annotations.FinishMethod
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FinishMethod(finishMethod)
Parameters: finishMethod ( NXOpen.Annotations.FinishMethod
) – New finish methodNew in version NX4.0.0.
License requirements: None.
GrooveAngle¶
-
LineWeldSideData.
GrooveAngle
¶ Returns or sets the groove angle
-------------------------------------
Getter Method
Signature
GrooveAngle()
Returns: Groove angle Return type: str New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GrooveAngle(grooveAngle)
Parameters: grooveAngle (str) – New groove angle New in version NX4.0.0.
License requirements: None.
LengthPitch¶
-
LineWeldSideData.
LengthPitch
¶ Returns or sets the weld length and pitch
-------------------------------------
Getter Method
Signature
LengthPitch()
Returns: Weld length and pitch Return type: str New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LengthPitch(lengthPitch)
Parameters: lengthPitch (str) – New weld length and pitch New in version NX4.0.0.
License requirements: None.
Size¶
-
LineWeldSideData.
Size
¶ Returns or sets the weld size
-------------------------------------
Getter Method
Signature
Size()
Returns: Weld size Return type: str New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Size(size)
Parameters: size (str) – New weld size New in version NX4.0.0.
License requirements: None.
SizeLetterCode¶
-
LineWeldSideData.
SizeLetterCode
¶ Returns or sets the weld size letter code (ISO and DIN only)
-------------------------------------
Getter Method
Signature
SizeLetterCode()
Returns: Size letter code Return type: NXOpen.Annotations.SizeLetterCode
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SizeLetterCode(sizeLetterCode)
Parameters: sizeLetterCode ( NXOpen.Annotations.SizeLetterCode
) – New size letter codeNew in version NX4.0.0.
License requirements: None.
SupplementarySymbol¶
-
LineWeldSideData.
SupplementarySymbol
¶ Returns or sets the weld supplementary symbol
-------------------------------------
Getter Method
Signature
SupplementarySymbol()
Returns: Supplementary weld symbol Return type: NXOpen.Annotations.SupplementarySymbol
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SupplementarySymbol(supplementarySymbol)
Parameters: supplementarySymbol ( NXOpen.Annotations.SupplementarySymbol
) – New supplementary weld symbolNew in version NX4.0.0.
License requirements: None.
Symbol¶
-
LineWeldSideData.
Symbol
¶ Returns or sets the elementary weld symbol
-------------------------------------
Getter Method
Signature
Symbol()
Returns: Weld symbol Return type: NXOpen.Annotations.Symbol
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Symbol(symbol)
Parameters: symbol ( NXOpen.Annotations.Symbol
) – New weld symbolNew in version NX4.0.0.
License requirements: None.