LineArrowStyleBuilder Class¶
-
class
NXOpen.Annotations.
LineArrowStyleBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.LineArrowStyleBuilder
.This class queries and sets preferences that apply to leaders and arrow and extension lines when creating or editing annotations, including dimensions.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AllAroundSymbolSize | Returns or sets the size of all around symbol. |
ArrowheadIncludedAngle | Returns or sets the arrowhead included angle |
ArrowheadLength | Returns or sets the arrowhead length |
ClipOrdinateDimensionLine | Returns or sets the clipping of the dimension line to the ordinate origin at the view border |
DatumLengthPastArrow | Returns or sets the distance from the apex of the datum arrowhead to the end of the extension line |
DotArrowheadDiameter | Returns or sets the dot arrowhead diameter |
FirstArrowLineColor | Returns or sets the first arrow line color |
FirstArrowLineFont | Returns or sets the first arrow line font |
FirstArrowLineWidth | Returns or sets the first arrow line width |
FirstArrowType | Returns or sets the first arrowhead type |
FirstArrowheadColor | Returns or sets the first arrowhead color |
FirstArrowheadFont | Returns or sets the first arrowhead font |
FirstArrowheadWidth | Returns or sets the first arrowhead width |
FirstExtensionLineColor | Returns or sets the first extension line color |
FirstExtensionLineFont | Returns or sets the first extension line font |
FirstExtensionLineWidth | Returns or sets the first extension line width |
FirstJogAngle | Returns or sets the first jog angle, between the jog and the extension line, in degrees. |
FirstJogDisplay | Returns or sets the first jog’s display flag, if true, the first jog will be displayed, false otherwise |
FirstJogEndOffset | Returns or sets the first jog end offset from the dimension line |
FirstJogOrientation | Returns or sets the first jog orientation, can be either IN or OUT |
FirstJogStartOffset | Returns or sets the first jog start offset from the dimension line |
FirstPosToExtensionLineDistance | Returns or sets the distance from the position on the object being dimensioned to the end of the first extension line or arc |
LeaderLocation | Returns or sets the leader location |
LeaderOrientation | Returns or sets the leader orientation |
LinePastArrowDistance | Returns or sets the distance an extension line or arc extends past the dimension line or arc |
LinePastArrowDistance2 | Returns or sets the second distance an extension line or arc extends past the dimension line or arc |
ObliqueExtensionLineAngle | Returns or sets the extension line angle. |
SecondArrowLineColor | Returns or sets the second arrow line color |
SecondArrowLineFont | Returns or sets the second arrow line font |
SecondArrowLineWidth | Returns or sets the second arrow line width |
SecondArrowType | Returns or sets the second arrowhead type |
SecondArrowheadColor | Returns or sets the second arrowhead color |
SecondArrowheadFont | Returns or sets the second arrowhead font |
SecondArrowheadWidth | Returns or sets the second arrowhead width |
SecondExtensionLineColor | Returns or sets the second extension line color |
SecondExtensionLineFont | Returns or sets the second extension line font |
SecondExtensionLineWidth | Returns or sets the second extension line width |
SecondJogAngle | Returns or sets the second jog angle, between the jog and the extension line, in degrees. |
SecondJogDisplay | Returns or sets the second jog’s display flag, if true, the second jog will be displayed, false otherwise |
SecondJogEndOffset | Returns or sets the second jog end offset from the dimension line |
SecondJogOrientation | Returns or sets the second jog orientation, can be either IN or OUT |
SecondJogStartOffset | Returns or sets the second jog start offset from the dimension line |
SecondPosToExtensionLineDistance | Returns or sets the distance from the position on the object being dimensioned to the end of the second extension line |
StubLength | Returns or sets the stub length. |
Tag | Returns the Tag for this object. |
TextOverLeaderGapFactor | Returns or sets the character size factor that controls the gap between text and the leader |
TextOverStubFactor | Returns or sets the character size factor which controls the distance between the stub and label text when the text displays above the stub line |
TextToLineDistance | Returns or sets the distance from the text to the dimension line(stub) or arc |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AllAroundSymbolSize¶
-
LineArrowStyleBuilder.
AllAroundSymbolSize
¶ Returns or sets the size of all around symbol.
This is also used for inner diameter of all over symbol
-------------------------------------
Getter Method
Signature
AllAroundSymbolSize()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AllAroundSymbolSize(allAroundSymbol)
Parameters: allAroundSymbol (float) – New in version NX8.5.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
ArrowheadIncludedAngle¶
-
LineArrowStyleBuilder.
ArrowheadIncludedAngle
¶ Returns or sets the arrowhead included angle
-------------------------------------
Getter Method
Signature
ArrowheadIncludedAngle()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ArrowheadIncludedAngle(arrowheadIncludedAngle)
Parameters: arrowheadIncludedAngle (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
ArrowheadLength¶
-
LineArrowStyleBuilder.
ArrowheadLength
¶ Returns or sets the arrowhead length
-------------------------------------
Getter Method
Signature
ArrowheadLength()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ArrowheadLength(arrowheadLength)
Parameters: arrowheadLength (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
ClipOrdinateDimensionLine¶
-
LineArrowStyleBuilder.
ClipOrdinateDimensionLine
¶ Returns or sets the clipping of the dimension line to the ordinate origin at the view border
-------------------------------------
Getter Method
Signature
ClipOrdinateDimensionLine()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClipOrdinateDimensionLine(clipOrdinateDimLine)
Parameters: clipOrdinateDimLine (bool) – New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
DatumLengthPastArrow¶
-
LineArrowStyleBuilder.
DatumLengthPastArrow
¶ Returns or sets the distance from the apex of the datum arrowhead to the end of the extension line
-------------------------------------
Getter Method
Signature
DatumLengthPastArrow()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DatumLengthPastArrow(datumLengthPastArrow)
Parameters: datumLengthPastArrow (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
DotArrowheadDiameter¶
-
LineArrowStyleBuilder.
DotArrowheadDiameter
¶ Returns or sets the dot arrowhead diameter
-------------------------------------
Getter Method
Signature
DotArrowheadDiameter()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DotArrowheadDiameter(dotArrowheadDiameter)
Parameters: dotArrowheadDiameter (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstArrowLineColor¶
-
LineArrowStyleBuilder.
FirstArrowLineColor
¶ Returns or sets the first arrow line color
-------------------------------------
Getter Method
Signature
FirstArrowLineColor()
Returns: Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstArrowLineColor(firstArrowLineColor)
Parameters: firstArrowLineColor (Id) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstArrowLineFont¶
-
LineArrowStyleBuilder.
FirstArrowLineFont
¶ Returns or sets the first arrow line font
-------------------------------------
Getter Method
Signature
FirstArrowLineFont()
Returns: Return type: NXOpen.DisplayableObjectObjectFont
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstArrowLineFont(firstArrowLineFont)
Parameters: firstArrowLineFont ( NXOpen.DisplayableObjectObjectFont
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstArrowLineWidth¶
-
LineArrowStyleBuilder.
FirstArrowLineWidth
¶ Returns or sets the first arrow line width
-------------------------------------
Getter Method
Signature
FirstArrowLineWidth()
Returns: Return type: NXOpen.Annotations.LineWidth
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstArrowLineWidth(firstArrowLineWidth)
Parameters: firstArrowLineWidth ( NXOpen.Annotations.LineWidth
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstArrowType¶
-
LineArrowStyleBuilder.
FirstArrowType
¶ Returns or sets the first arrowhead type
-------------------------------------
Getter Method
Signature
FirstArrowType()
Returns: Return type: NXOpen.Annotations.ArrowheadType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstArrowType(firstArrowType)
Parameters: firstArrowType ( NXOpen.Annotations.ArrowheadType
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstArrowheadColor¶
-
LineArrowStyleBuilder.
FirstArrowheadColor
¶ Returns or sets the first arrowhead color
-------------------------------------
Getter Method
Signature
FirstArrowheadColor()
Returns: Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstArrowheadColor(firstArrowheadColor)
Parameters: firstArrowheadColor (Id) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstArrowheadFont¶
-
LineArrowStyleBuilder.
FirstArrowheadFont
¶ Returns or sets the first arrowhead font
-------------------------------------
Getter Method
Signature
FirstArrowheadFont()
Returns: Return type: NXOpen.DisplayableObjectObjectFont
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstArrowheadFont(firstArrowheadFont)
Parameters: firstArrowheadFont ( NXOpen.DisplayableObjectObjectFont
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstArrowheadWidth¶
-
LineArrowStyleBuilder.
FirstArrowheadWidth
¶ Returns or sets the first arrowhead width
-------------------------------------
Getter Method
Signature
FirstArrowheadWidth()
Returns: Return type: NXOpen.Annotations.LineWidth
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstArrowheadWidth(firstArrowheadWidth)
Parameters: firstArrowheadWidth ( NXOpen.Annotations.LineWidth
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstExtensionLineColor¶
-
LineArrowStyleBuilder.
FirstExtensionLineColor
¶ Returns or sets the first extension line color
-------------------------------------
Getter Method
Signature
FirstExtensionLineColor()
Returns: Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstExtensionLineColor(firstExtensionLineColor)
Parameters: firstExtensionLineColor (Id) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstExtensionLineFont¶
-
LineArrowStyleBuilder.
FirstExtensionLineFont
¶ Returns or sets the first extension line font
-------------------------------------
Getter Method
Signature
FirstExtensionLineFont()
Returns: Return type: NXOpen.DisplayableObjectObjectFont
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstExtensionLineFont(firstExtensionLineFont)
Parameters: firstExtensionLineFont ( NXOpen.DisplayableObjectObjectFont
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstExtensionLineWidth¶
-
LineArrowStyleBuilder.
FirstExtensionLineWidth
¶ Returns or sets the first extension line width
-------------------------------------
Getter Method
Signature
FirstExtensionLineWidth()
Returns: Return type: NXOpen.Annotations.LineWidth
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstExtensionLineWidth(firstExtensionLineWidth)
Parameters: firstExtensionLineWidth ( NXOpen.Annotations.LineWidth
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstJogAngle¶
-
LineArrowStyleBuilder.
FirstJogAngle
¶ Returns or sets the first jog angle, between the jog and the extension line, in degrees.
-------------------------------------
Getter Method
Signature
FirstJogAngle()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstJogAngle(jogAngle)
Parameters: jogAngle (float) – New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstJogDisplay¶
-
LineArrowStyleBuilder.
FirstJogDisplay
¶ Returns or sets the first jog’s display flag, if true, the first jog will be displayed, false otherwise
-------------------------------------
Getter Method
Signature
FirstJogDisplay()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstJogDisplay(jogDisplay)
Parameters: jogDisplay (bool) – New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstJogEndOffset¶
-
LineArrowStyleBuilder.
FirstJogEndOffset
¶ Returns or sets the first jog end offset from the dimension line
-------------------------------------
Getter Method
Signature
FirstJogEndOffset()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstJogEndOffset(jogEndOffset)
Parameters: jogEndOffset (float) – New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstJogOrientation¶
-
LineArrowStyleBuilder.
FirstJogOrientation
¶ Returns or sets the first jog orientation, can be either IN or OUT
-------------------------------------
Getter Method
Signature
FirstJogOrientation()
Returns: Return type: NXOpen.Annotations.JogOrientation
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstJogOrientation(jogOrientation)
Parameters: jogOrientation ( NXOpen.Annotations.JogOrientation
) –New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstJogStartOffset¶
-
LineArrowStyleBuilder.
FirstJogStartOffset
¶ Returns or sets the first jog start offset from the dimension line
-------------------------------------
Getter Method
Signature
FirstJogStartOffset()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstJogStartOffset(jogStartOffset)
Parameters: jogStartOffset (float) – New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstPosToExtensionLineDistance¶
-
LineArrowStyleBuilder.
FirstPosToExtensionLineDistance
¶ Returns or sets the distance from the position on the object being dimensioned to the end of the first extension line or arc
-------------------------------------
Getter Method
Signature
FirstPosToExtensionLineDistance()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstPosToExtensionLineDistance(firstPosToExtensionLineDistance)
Parameters: firstPosToExtensionLineDistance (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
LeaderLocation¶
-
LineArrowStyleBuilder.
LeaderLocation
¶ Returns or sets the leader location
-------------------------------------
Getter Method
Signature
LeaderLocation()
Returns: Return type: NXOpen.Annotations.VerticalTextJustification
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LeaderLocation(leaderLocation)
Parameters: leaderLocation ( NXOpen.Annotations.VerticalTextJustification
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
LeaderOrientation¶
-
LineArrowStyleBuilder.
LeaderOrientation
¶ Returns or sets the leader orientation
-------------------------------------
Getter Method
Signature
LeaderOrientation()
Returns: Return type: NXOpen.Annotations.LeaderSide
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LeaderOrientation(leaderOrientation)
Parameters: leaderOrientation ( NXOpen.Annotations.LeaderSide
) –New in version NX9.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
LinePastArrowDistance¶
-
LineArrowStyleBuilder.
LinePastArrowDistance
¶ Returns or sets the distance an extension line or arc extends past the dimension line or arc
-------------------------------------
Getter Method
Signature
LinePastArrowDistance()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LinePastArrowDistance(linePastArrowDistance)
Parameters: linePastArrowDistance (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
LinePastArrowDistance2¶
-
LineArrowStyleBuilder.
LinePastArrowDistance2
¶ Returns or sets the second distance an extension line or arc extends past the dimension line or arc
-------------------------------------
Getter Method
Signature
LinePastArrowDistance2()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LinePastArrowDistance2(linePastArrowDistance)
Parameters: linePastArrowDistance (float) – New in version NX9.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
ObliqueExtensionLineAngle¶
-
LineArrowStyleBuilder.
ObliqueExtensionLineAngle
¶ Returns or sets the extension line angle.
This angle only applies to vertical and horizontal dimensions
-------------------------------------
Getter Method
Signature
ObliqueExtensionLineAngle()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ObliqueExtensionLineAngle(obliqueExtensionLineAngle)
Parameters: obliqueExtensionLineAngle (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondArrowLineColor¶
-
LineArrowStyleBuilder.
SecondArrowLineColor
¶ Returns or sets the second arrow line color
-------------------------------------
Getter Method
Signature
SecondArrowLineColor()
Returns: Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondArrowLineColor(secondArrowLineColor)
Parameters: secondArrowLineColor (Id) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondArrowLineFont¶
-
LineArrowStyleBuilder.
SecondArrowLineFont
¶ Returns or sets the second arrow line font
-------------------------------------
Getter Method
Signature
SecondArrowLineFont()
Returns: Return type: NXOpen.DisplayableObjectObjectFont
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondArrowLineFont(secondArrowLineFont)
Parameters: secondArrowLineFont ( NXOpen.DisplayableObjectObjectFont
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondArrowLineWidth¶
-
LineArrowStyleBuilder.
SecondArrowLineWidth
¶ Returns or sets the second arrow line width
-------------------------------------
Getter Method
Signature
SecondArrowLineWidth()
Returns: Return type: NXOpen.Annotations.LineWidth
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondArrowLineWidth(secondArrowLineWidth)
Parameters: secondArrowLineWidth ( NXOpen.Annotations.LineWidth
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondArrowType¶
-
LineArrowStyleBuilder.
SecondArrowType
¶ Returns or sets the second arrowhead type
-------------------------------------
Getter Method
Signature
SecondArrowType()
Returns: Return type: NXOpen.Annotations.ArrowheadType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondArrowType(secondArrowType)
Parameters: secondArrowType ( NXOpen.Annotations.ArrowheadType
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondArrowheadColor¶
-
LineArrowStyleBuilder.
SecondArrowheadColor
¶ Returns or sets the second arrowhead color
-------------------------------------
Getter Method
Signature
SecondArrowheadColor()
Returns: Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondArrowheadColor(secondArrowheadColor)
Parameters: secondArrowheadColor (Id) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondArrowheadFont¶
-
LineArrowStyleBuilder.
SecondArrowheadFont
¶ Returns or sets the second arrowhead font
-------------------------------------
Getter Method
Signature
SecondArrowheadFont()
Returns: Return type: NXOpen.DisplayableObjectObjectFont
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondArrowheadFont(secondArrowheadFont)
Parameters: secondArrowheadFont ( NXOpen.DisplayableObjectObjectFont
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondArrowheadWidth¶
-
LineArrowStyleBuilder.
SecondArrowheadWidth
¶ Returns or sets the second arrowhead width
-------------------------------------
Getter Method
Signature
SecondArrowheadWidth()
Returns: Return type: NXOpen.Annotations.LineWidth
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondArrowheadWidth(secondArrowheadWidth)
Parameters: secondArrowheadWidth ( NXOpen.Annotations.LineWidth
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondExtensionLineColor¶
-
LineArrowStyleBuilder.
SecondExtensionLineColor
¶ Returns or sets the second extension line color
-------------------------------------
Getter Method
Signature
SecondExtensionLineColor()
Returns: Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondExtensionLineColor(secondExtensionLineColor)
Parameters: secondExtensionLineColor (Id) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondExtensionLineFont¶
-
LineArrowStyleBuilder.
SecondExtensionLineFont
¶ Returns or sets the second extension line font
-------------------------------------
Getter Method
Signature
SecondExtensionLineFont()
Returns: Return type: NXOpen.DisplayableObjectObjectFont
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondExtensionLineFont(secondExtensionLineFont)
Parameters: secondExtensionLineFont ( NXOpen.DisplayableObjectObjectFont
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondExtensionLineWidth¶
-
LineArrowStyleBuilder.
SecondExtensionLineWidth
¶ Returns or sets the second extension line width
-------------------------------------
Getter Method
Signature
SecondExtensionLineWidth()
Returns: Return type: NXOpen.Annotations.LineWidth
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondExtensionLineWidth(secondExtensionLineWidth)
Parameters: secondExtensionLineWidth ( NXOpen.Annotations.LineWidth
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondJogAngle¶
-
LineArrowStyleBuilder.
SecondJogAngle
¶ Returns or sets the second jog angle, between the jog and the extension line, in degrees.
-------------------------------------
Getter Method
Signature
SecondJogAngle()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondJogAngle(jogAngle)
Parameters: jogAngle (float) – New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondJogDisplay¶
-
LineArrowStyleBuilder.
SecondJogDisplay
¶ Returns or sets the second jog’s display flag, if true, the second jog will be displayed, false otherwise
-------------------------------------
Getter Method
Signature
SecondJogDisplay()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondJogDisplay(jogDisplay)
Parameters: jogDisplay (bool) – New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondJogEndOffset¶
-
LineArrowStyleBuilder.
SecondJogEndOffset
¶ Returns or sets the second jog end offset from the dimension line
-------------------------------------
Getter Method
Signature
SecondJogEndOffset()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondJogEndOffset(jogEndOffset)
Parameters: jogEndOffset (float) – New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondJogOrientation¶
-
LineArrowStyleBuilder.
SecondJogOrientation
¶ Returns or sets the second jog orientation, can be either IN or OUT
-------------------------------------
Getter Method
Signature
SecondJogOrientation()
Returns: Return type: NXOpen.Annotations.JogOrientation
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondJogOrientation(jogOrientation)
Parameters: jogOrientation ( NXOpen.Annotations.JogOrientation
) –New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondJogStartOffset¶
-
LineArrowStyleBuilder.
SecondJogStartOffset
¶ Returns or sets the second jog start offset from the dimension line
-------------------------------------
Getter Method
Signature
SecondJogStartOffset()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondJogStartOffset(jogStartOffset)
Parameters: jogStartOffset (float) – New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondPosToExtensionLineDistance¶
-
LineArrowStyleBuilder.
SecondPosToExtensionLineDistance
¶ Returns or sets the distance from the position on the object being dimensioned to the end of the second extension line
-------------------------------------
Getter Method
Signature
SecondPosToExtensionLineDistance()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondPosToExtensionLineDistance(secondPosToExtensionLineDistance)
Parameters: secondPosToExtensionLineDistance (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
StubLength¶
-
LineArrowStyleBuilder.
StubLength
¶ Returns or sets the stub length.
This is the size of the dogleg on a label or dimension
-------------------------------------
Getter Method
Signature
StubLength()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StubLength(stubLength)
Parameters: stubLength (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
TextOverLeaderGapFactor¶
-
LineArrowStyleBuilder.
TextOverLeaderGapFactor
¶ Returns or sets the character size factor that controls the gap between text and the leader
-------------------------------------
Getter Method
Signature
TextOverLeaderGapFactor()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TextOverLeaderGapFactor(textOverLeaderGapFactor)
Parameters: textOverLeaderGapFactor (float) – New in version NX8.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
TextOverStubFactor¶
-
LineArrowStyleBuilder.
TextOverStubFactor
¶ Returns or sets the character size factor which controls the distance between the stub and label text when the text displays above the stub line
-------------------------------------
Getter Method
Signature
TextOverStubFactor()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TextOverStubFactor(textOverStubFactor)
Parameters: textOverStubFactor (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
TextToLineDistance¶
-
LineArrowStyleBuilder.
TextToLineDistance
¶ Returns or sets the distance from the text to the dimension line(stub) or arc
-------------------------------------
Getter Method
Signature
TextToLineDistance()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TextToLineDistance(textToLineDistance)
Parameters: textToLineDistance (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
LineArrowStyleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.