IntersectionSymbolCollection Class¶
-
class
NXOpen.Annotations.
IntersectionSymbolCollection
¶ Bases:
object
Represents a collection of
NXOpen.Annotations.IntersectionSymbol
objectsTo obtain an instance of this class, refer to
NXOpen.Annotations.AnnotationManager
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreateIntersectionSymbolBuilder | Creates the IntersectionSymbolBuilder @return IntersectionSymbolBuilder object |
FindObject | Finds the intersection symbol with the given name. |
Method Detail¶
CreateIntersectionSymbolBuilder¶
-
IntersectionSymbolCollection.
CreateIntersectionSymbolBuilder
¶ Creates the IntersectionSymbolBuilder
Signature
CreateIntersectionSymbolBuilder(intersectionPt)
Parameters: intersectionPt ( NXOpen.Annotations.IntersectionSymbol
) –NXOpen.Annotations.IntersectionSymbol
to be edited, if None then create a new oneReturns: IntersectionSymbolBuilder object Return type: NXOpen.Annotations.IntersectionSymbolBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
FindObject¶
-
IntersectionSymbolCollection.
FindObject
¶ Finds the intersection symbol with the given name.
An exception will be thrown if no object can be found with given name
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier of the intersection symbol to be found Returns: Intersecton Symbol with this identifier Return type: NXOpen.Annotations.IntersectionSymbol
New in version NX6.0.0.
License requirements: None.