ImportSymbolBuilder Class¶
-
class
NXOpen.Annotations.
ImportSymbolBuilder
¶ Bases:
NXOpen.Builder
Represents a builder allowing import of one or many foreign symbols.
To create a new instance of this class, use
NXOpen.DraftingManager.CreateImportSymbolBuilder
Default values.
Property Value IncludeSubfolders 0 PreserveFolderStructure 0 SelectMode File New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
IncludeSubfolders | Returns or sets the subfolders toggle |
InputFolder | Returns or sets the name of the input folder |
IsPartSymbol | Returns or sets the Is Part Symbol status |
IsTeamcenter | Returns or sets the Teamcwenter mode status |
LibraryPath | Returns or sets the Reuse library path selection |
PreserveFolderStructure | Returns or sets the folder structure toggle |
SelectMode | Returns or sets the selection mode |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetExpandedFiles | Returns the names of the expanded files |
GetFilesToProcess | Returns the names of the selected files |
GetObject | Returns the object currently being edited by this builder. |
SetExpandedFiles | Sets the names of the expanded files |
SetFilesToProcess | Sets the names of the selected files |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
StartImport | Starts the Import process |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ImportSymbolBuilderFileFolder Enumeration | the Selection mode Enum |
Property Detail¶
IncludeSubfolders¶
-
ImportSymbolBuilder.
IncludeSubfolders
¶ Returns or sets the subfolders toggle
-------------------------------------
Getter Method
Signature
IncludeSubfolders()
Returns: Return type: bool New in version NX7.5.0.
License requirements: nx_layout (“NX Layout”)
-------------------------------------
Setter Method
Signature
IncludeSubfolders(includeSubfolders)
Parameters: includeSubfolders (bool) – New in version NX7.5.0.
License requirements: nx_layout (“NX Layout”)
InputFolder¶
-
ImportSymbolBuilder.
InputFolder
¶ Returns or sets the name of the input folder
-------------------------------------
Getter Method
Signature
InputFolder()
Returns: Return type: str New in version NX7.5.0.
License requirements: nx_layout (“NX Layout”)
-------------------------------------
Setter Method
Signature
InputFolder(foldername)
Parameters: foldername (str) – New in version NX7.5.0.
License requirements: nx_layout (“NX Layout”)
IsPartSymbol¶
-
ImportSymbolBuilder.
IsPartSymbol
¶ Returns or sets the Is Part Symbol status
-------------------------------------
Getter Method
Signature
IsPartSymbol()
Returns: Return type: bool New in version NX7.5.0.
License requirements: nx_layout (“NX Layout”)
-------------------------------------
Setter Method
Signature
IsPartSymbol(isPartSymbol)
Parameters: isPartSymbol (bool) – New in version NX7.5.0.
License requirements: nx_layout (“NX Layout”)
IsTeamcenter¶
-
ImportSymbolBuilder.
IsTeamcenter
¶ Returns or sets the Teamcwenter mode status
-------------------------------------
Getter Method
Signature
IsTeamcenter()
Returns: Return type: bool New in version NX7.5.0.
License requirements: nx_layout (“NX Layout”)
-------------------------------------
Setter Method
Signature
IsTeamcenter(isTeamcenter)
Parameters: isTeamcenter (bool) – New in version NX7.5.0.
License requirements: nx_layout (“NX Layout”)
LibraryPath¶
-
ImportSymbolBuilder.
LibraryPath
¶ Returns or sets the Reuse library path selection
-------------------------------------
Getter Method
Signature
LibraryPath()
Returns: Return type: str New in version NX7.5.0.
License requirements: nx_layout (“NX Layout”)
-------------------------------------
Setter Method
Signature
LibraryPath(path)
Parameters: path (str) – New in version NX7.5.0.
License requirements: nx_layout (“NX Layout”)
PreserveFolderStructure¶
-
ImportSymbolBuilder.
PreserveFolderStructure
¶ Returns or sets the folder structure toggle
-------------------------------------
Getter Method
Signature
PreserveFolderStructure()
Returns: Return type: bool New in version NX7.5.0.
License requirements: nx_layout (“NX Layout”)
-------------------------------------
Setter Method
Signature
PreserveFolderStructure(preserveFolderStructure)
Parameters: preserveFolderStructure (bool) – New in version NX7.5.0.
License requirements: nx_layout (“NX Layout”)
SelectMode¶
-
ImportSymbolBuilder.
SelectMode
¶ Returns or sets the selection mode
-------------------------------------
Getter Method
Signature
SelectMode()
Returns: Return type: NXOpen.Annotations.ImportSymbolBuilderFileFolder
New in version NX7.5.0.
License requirements: nx_layout (“NX Layout”)
-------------------------------------
Setter Method
Signature
SelectMode(selectMode)
Parameters: selectMode ( NXOpen.Annotations.ImportSymbolBuilderFileFolder
) –New in version NX7.5.0.
License requirements: nx_layout (“NX Layout”)
Method Detail¶
GetExpandedFiles¶
-
ImportSymbolBuilder.
GetExpandedFiles
¶ Returns the names of the expanded files
Signature
GetExpandedFiles()
Returns: the list of selected files Return type: list of str New in version NX7.5.0.
License requirements: nx_layout (“NX Layout”)
GetFilesToProcess¶
-
ImportSymbolBuilder.
GetFilesToProcess
¶ Returns the names of the selected files
Signature
GetFilesToProcess()
Returns: the list of selected files Return type: list of str New in version NX7.5.0.
License requirements: nx_layout (“NX Layout”)
SetExpandedFiles¶
-
ImportSymbolBuilder.
SetExpandedFiles
¶ Sets the names of the expanded files
Signature
SetExpandedFiles(files)
Parameters: files (list of str) – the list of the selected files NOTE: The full Unicode character set is not supported for this parameter. New in version NX7.5.0.
License requirements: nx_layout (“NX Layout”)
SetFilesToProcess¶
-
ImportSymbolBuilder.
SetFilesToProcess
¶ Sets the names of the selected files
Signature
SetFilesToProcess(files)
Parameters: files (list of str) – the list of the selected files NOTE: The full Unicode character set is not supported for this parameter. New in version NX7.5.0.
License requirements: nx_layout (“NX Layout”)
StartImport¶
-
ImportSymbolBuilder.
StartImport
¶ Starts the Import process
Signature
StartImport()
New in version NX7.5.0.
License requirements: nx_layout (“NX Layout”)
Validate¶
-
ImportSymbolBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.