IdentificationLineLocation Enumeration¶
-
class
NXOpen.Annotations.
IdentificationLineLocation
¶ Bases:
object
Specifies the weld identification line location (ISO and DIN only) Enum Members
- reference line “
- “Bottom”, ” Specifies identification line below the
- reference line “
- “Last”, ” Last enum value. Should not be used. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.