HoleCalloutSettingsBuilderParametertype Enumeration¶
NXOpen.Annotations.HoleCalloutSettingsBuilder.Parametertype is an alias for NXOpen.Annotations.HoleCalloutSettingsBuilderParametertype
-
class
NXOpen.Annotations.
HoleCalloutSettingsBuilderParametertype
¶ Bases:
object
This reprensent the option that indicates a type of hole feature parameters.
Enum Members
Enum Member Enum Member Description Diameter Depth CounterBoreDiameter CounterBoreDepth CounterSinkDiameter CounterSinkAngle TaperAngle PatternFeatureCount ScrewSize Fit LineBreak ThreadSize ThreadDepth Pitch Angle MinorDiameter MajorDiameter TapDrillDiameter Callout Length ShaftSize None -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-