HatchFillSettingsBuilder Class¶
-
class
NXOpen.Annotations.
HatchFillSettingsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
This class is used to construct the Crosshatch and area Fill setting block .
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Angle | Returns or sets the angle |
AnnotationType | Returns or sets the type of hatch object |
AreafillAngle | Returns or sets the areafill angle |
Color | Returns or sets the color |
CrosshatchFile | Returns or sets the crosshatch file |
Distance | Returns or sets the distance |
Material | Returns or sets the area fill material |
Pattern | Returns or sets the pattern |
Scale | Returns or sets the scale |
Tag | Returns the Tag for this object. |
Tolerance | Returns or sets the tolerance |
Width | Returns or sets the width |
Methods¶
Method | Description |
---|---|
FindCrosshatchFile | Finds the crosshatch file from pattern. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
HatchFillSettingsBuilderAnnotationTypes Enumeration | the valid types of hatch objects |
Property Detail¶
Angle¶
-
HatchFillSettingsBuilder.
Angle
¶ Returns or sets the angle
-------------------------------------
Getter Method
Signature
Angle()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Angle(angle)
Parameters: angle (float) – New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
AnnotationType¶
-
HatchFillSettingsBuilder.
AnnotationType
¶ Returns or sets the type of hatch object
-------------------------------------
Getter Method
Signature
AnnotationType()
Returns: Return type: NXOpen.Annotations.HatchFillSettingsBuilderAnnotationTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AnnotationType(type)
Parameters: type ( NXOpen.Annotations.HatchFillSettingsBuilderAnnotationTypes
) –New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
AreafillAngle¶
-
HatchFillSettingsBuilder.
AreafillAngle
¶ Returns or sets the areafill angle
-------------------------------------
Getter Method
Signature
AreafillAngle()
Returns: Return type: float New in version NX6.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
AreafillAngle(angle)
Parameters: angle (float) – New in version NX6.0.1.
License requirements: drafting (“DRAFTING”)
Color¶
-
HatchFillSettingsBuilder.
Color
¶ Returns or sets the color
-------------------------------------
Getter Method
Signature
Color()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Color(color)
Parameters: color (Id) – New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
CrosshatchFile¶
-
HatchFillSettingsBuilder.
CrosshatchFile
¶ Returns or sets the crosshatch file
-------------------------------------
Getter Method
Signature
CrosshatchFile()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CrosshatchFile(filename)
Parameters: filename (str) – New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
Distance¶
-
HatchFillSettingsBuilder.
Distance
¶ Returns or sets the distance
-------------------------------------
Getter Method
Signature
Distance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Distance(distance)
Parameters: distance (float) – New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
Material¶
-
HatchFillSettingsBuilder.
Material
¶ Returns or sets the area fill material
-------------------------------------
Getter Method
Signature
Material()
Returns: Return type: NXOpen.Annotations.AreaFillMaterial
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Material(areaFillMaterial)
Parameters: areaFillMaterial ( NXOpen.Annotations.AreaFillMaterial
) –New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
Pattern¶
-
HatchFillSettingsBuilder.
Pattern
¶ Returns or sets the pattern
-------------------------------------
Getter Method
Signature
Pattern()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Pattern(identifier)
Parameters: identifier (str) – New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
Scale¶
-
HatchFillSettingsBuilder.
Scale
¶ Returns or sets the scale
-------------------------------------
Getter Method
Signature
Scale()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Scale(scale)
Parameters: scale (float) – New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Tolerance¶
-
HatchFillSettingsBuilder.
Tolerance
¶ Returns or sets the tolerance
-------------------------------------
Getter Method
Signature
Tolerance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance(tolerance)
Parameters: tolerance (float) – New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
Width¶
-
HatchFillSettingsBuilder.
Width
¶ Returns or sets the width
-------------------------------------
Getter Method
Signature
Width()
Returns: Return type: NXOpen.Annotations.LineWidth
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width(width)
Parameters: width ( NXOpen.Annotations.LineWidth
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
FindCrosshatchFile¶
-
HatchFillSettingsBuilder.
FindCrosshatchFile
¶ Finds the crosshatch file from pattern.
May be blank if not found
Signature
FindCrosshatchFile(identifier)
Parameters: identifier (str) – Returns: Return type: str New in version NX8.5.0.
License requirements: None.
Validate¶
-
HatchFillSettingsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.