HatchBuilderAnnotationTypes Enumeration¶
NXOpen.Annotations.HatchBuilder.AnnotationTypes is an alias for NXOpen.Annotations.HatchBuilderAnnotationTypes
-
class
NXOpen.Annotations.
HatchBuilderAnnotationTypes
¶ Bases:
object
Represents types of hatch objects.
Use
NXOpen.Annotations.HatchBuilder.HatchFillSettings
instead.. .. deprecated:: NX7.5.0UseNXOpen.Annotations.HatchBuilder.HatchFillSettings
instead.Enum Members
Enum Member Enum Member Description Crosshatch CrosshatchAreaFill Area Fill-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-