FrameBarBuilder Class¶
-
class
NXOpen.Annotations.
FrameBarBuilder
¶ Bases:
NXOpen.Annotations.BaseFrameBarBuilder
Represents a
NXOpen.Annotations.FrameBarBuilder
.This class allows to create frame bar annotation
To create a new instance of this class, use
NXOpen.Annotations.FrameBarCollection.CreateFrameBarBuilder
Default values.
Property Value AftPerpendicular 0 Axis X Baseline 0 BulkHeads 0 Centerline 0 Decks 0 ForwardPerpendicular 0 InterTransverseFrames 0 LongitudinalYFrames 0 LongitudinalZFrames 0 TransveralInsertArea 0 TransverseFrames 0 Waterline 0 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AftPerpendicular | Returns or sets the aft perpendicular |
Axis | Returns or sets the axis |
Baseline | Returns or sets the baseline |
BulkHeads | Returns or sets the bulk heads |
Centerline | Returns or sets the centerline |
Decks | Returns or sets the decks |
ForwardPerpendicular | Returns or sets the forward perpendicular |
InterTransverseFrames | Returns or sets the inter transverse frames |
LongitudinalYFrames | Returns or sets the longitudinal yframes |
LongitudinalZFrames | Returns or sets the longitudinal zframes |
Origin | Returns the origin |
Style | Returns the style |
Tag | Returns the Tag for this object. |
TransveralInsertArea | Returns or sets the transveral insert area |
TransverseFrames | Returns or sets the transverse frames |
View | Returns the select view |
Waterline | Returns or sets the waterline |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateFrameBarObject | Creates frame bar object |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFramebar | The frame bar @return The frame bar |
GetObject | Returns the object currently being edited by this builder. |
ReverseTics | This function is used to reverse tics on the framebar |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateFrameBarFromStyle | Updates frame bar object as per style |
UpdateFromConceptModel | This function is used to update framebar from Concept model |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
Validate¶
-
FrameBarBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.