FlipOption Enumeration¶
-
class
NXOpen.Annotations.
FlipOption
¶ Bases:
object
Specifies the custom symbol flip option.
This option is only available when editing. This option is unavailable for symbols with leaders. Enum Members
- line taken through its anchor point “
- “Vertical”, ” Flips a symbol vertically about a horizontal
- line taken through its anchor point “
- “Last”, ” Last enum value. Should not be used. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.