AreaSymbol |
Returns or sets the area symbol |
CircleU |
Returns or sets the circle utoggle |
CircleUvalue |
Returns or sets the circle u value Only available when Annotations.FeatureControlFrameDataBuilder.CircleU is true. |
CommonZone |
Returns or sets the common zone toggle |
FreeState |
Returns or sets the free state toggle |
MaterialModifier |
Returns or sets the material modifier |
MaximumTolerance |
Returns or sets the maximum tolerance toggle |
MaximumToleranceValue |
Returns or sets the maximum tolerance value Only available when Annotations.FeatureControlFrameDataBuilder.MaximumTolerance is true. |
PrimaryCompoundDatumReference |
Returns the primary compound datum reference |
PrimaryDatumExtendedText |
Returns or sets the primary datum extended text. |
PrimaryDatumReference |
Returns the primary datum reference |
Projected |
Returns or sets the projected toggle |
ProjectedValue |
Returns or sets the projected value Only available when Annotations.FeatureControlFrameDataBuilder.Projected is true. |
SecondaryCompoundDatumReference |
Returns the secondary compound datum reference |
SecondaryDatumExtendedText |
Returns or sets the secondary datum extended text. |
SecondaryDatumReference |
Returns the secondary datum reference |
StatisticalTolerance |
Returns or sets the statistical tolerance toggle |
Tag |
Returns the Tag for this object. |
TangentPlane |
Returns or sets the tangent plane toggle |
TertiaryCompoundDatumReference |
Returns the tertiary compound datum reference |
TertiaryDatumExtendedText |
Returns or sets the tertiary datum extended text. |
TertiaryDatumReference |
Returns the tertiary datum reference |
ToleranceValue |
Returns or sets the tolerance value string |
UnitBasis |
Returns or sets the unit basis toggle Only available when feature control frame characteristic is Annotations.FeatureControlFrameBuilderFcfCharacteristic.Straightness Annotations.FeatureControlFrameBuilderFcfCharacteristic.Flatness Annotations.FeatureControlFrameBuilderFcfCharacteristic.ProfileOfALine Annotations.FeatureControlFrameBuilderFcfCharacteristic.ProfileOfASurface |
UnitBasisValue1 |
Returns or sets the unit basis value1 Only available when Annotations.FeatureControlFrameDataBuilder.UnitBasis is true. |
UnitBasisValue2 |
Returns or sets the unit basis value2 Only available when Annotations.FeatureControlFrameDataBuilder.UnitBasis is true. |
ZoneShape |
Returns or sets the zone shape |