FeatureControlFrameBuilderFcfCharacteristic Enumeration¶
NXOpen.Annotations.FeatureControlFrameBuilder.FcfCharacteristic is an alias for NXOpen.Annotations.FeatureControlFrameBuilderFcfCharacteristic
-
class
NXOpen.Annotations.
FeatureControlFrameBuilderFcfCharacteristic
¶ Bases:
object
Specifies the characteristitic of the feature control frame
Enum Members
Enum Member Enum Member Description Straightness straightnessFlatness flatnessCircularity circularityCylindricity cylindricityProfileOfALine profile of a lineProfileOfASurface profile of a sufraceAngularity angularityPerpendicularity perpendicularityParallelism parallelismPosition positionConcentricity concentricitySymmetry symmetryCircularRunout circular runoutTotalRunout total runoutAxisIntersection axis intersection-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-