ExtensionLineDisplay Enumeration¶
-
class
NXOpen.Annotations.
ExtensionLineDisplay
¶ Bases:
object
Specifies the extension line display option Enum Members
- first object selected to create the dimension “
- “Second”, ” Displays extension line attached to the
- second object selected to create the dimension “
- “None”, ” Doesn’t display extension lines ” “Last”, ” Last enum value. Should not be used. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.