DualDimensionPlacement Enumeration¶
-
class
NXOpen.Annotations.
DualDimensionPlacement
¶ Bases:
object
Specifies the dual dimension placement relative to the primary dimension Enum Members
Enum Member Enum Member Description Below Specifies dual dimension below primary dimensionAfter Specifies dual dimension after primary dimensionAbove Specifies dual dimension above primary dimensionBefore Specifies dual dimension before primary dimensionNone Specifies no dual dimensionLast Last enum value. Should not be used.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-