DraftingNoteBuilderTextAlign Enumeration¶
NXOpen.Annotations.DraftingNoteBuilder.TextAlign is an alias for NXOpen.Annotations.DraftingNoteBuilderTextAlign
-
class
NXOpen.Annotations.
DraftingNoteBuilderTextAlign
¶ Bases:
object
text over leader types for text
Enum Members
Enum Member Enum Member Description Top Align topMiddle Align middleBottom Align bottomBelowbottomExtToMax Align below bottom extension to maximumBelowbottomExtToMaxUnderline Align below bottom extension to maximum and underlineBelowbottom Align below bottomBelowbottomUnderline Align below bottom and underlineBelowTopExtToMax Align below top extension to maximumBelowTopExtToMaxUnderline Align below top extension to maximum and underlineBelowTop Align below topBelowTopUnderline Align below top and underline-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-