DimensionWorkflowBuilder Class¶
-
class
NXOpen.Annotations.
DimensionWorkflowBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a Annotations WorkFlowBuilder.
This class queries and sets general dimension attributes while creating or editing a dimension.
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
EnableDirectedDimension | Returns or sets the directed dimension. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
EnableDirectedDimension¶
-
DimensionWorkflowBuilder.
EnableDirectedDimension
¶ Returns or sets the directed dimension.
This specifies whether to create directed dimension or not
-------------------------------------
Getter Method
Signature
EnableDirectedDimension()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnableDirectedDimension(directedDimension)
Parameters: directedDimension (bool) – New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
DimensionWorkflowBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.