DimensionSetBuilder Class¶
-
class
NXOpen.Annotations.
DimensionSetBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.DimensionSetBuilder
This is a sub-builder class and cannot be directly instantiated
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
DimensionOrSet | Returns the dimension or dimension set object |
Method | Returns or sets the dimension set method |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DimensionSetBuilderDimensionSetMethod Enumeration | dimension set method |
Property Detail¶
DimensionOrSet¶
-
DimensionSetBuilder.
DimensionOrSet
¶ Returns the dimension or dimension set object
-------------------------------------
Getter Method
Signature
DimensionOrSet()
Returns: Return type: NXOpen.Annotations.SelectAnnotation
New in version NX9.0.0.
License requirements: None.
Method¶
-
DimensionSetBuilder.
Method
¶ Returns or sets the dimension set method
-------------------------------------
Getter Method
Signature
Method()
Returns: Return type: NXOpen.Annotations.DimensionSetBuilderDimensionSetMethod
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Method(method)
Parameters: method ( NXOpen.Annotations.DimensionSetBuilderDimensionSetMethod
) –New in version NX9.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”) OR solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
DimensionSetBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.