DimensionMeasurementBuilderMeasurementMethod Enumeration¶
NXOpen.Annotations.DimensionMeasurementBuilder.MeasurementMethod is an alias for NXOpen.Annotations.DimensionMeasurementBuilderMeasurementMethod
-
class
NXOpen.Annotations.
DimensionMeasurementBuilderMeasurementMethod
¶ Bases:
object
measurement method for the dimensions
Enum Members
Enum Member Enum Member Description Inferred Inferred measurement direction (UI Only)Horizontal Horizontal measurement directionVertical Vertical measurement directionPointToPoint Point to point measurement directionPerpendicular Perpendicular measurement directionCylindrical Linear measurement method representing a diameterAngular Angular measurement typeRadial Radial measurement typeDiametral Diametral measurement typeHoleCallout Hole Callout based measurement-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-