CuttingPlaneSymbolBuilderViewNameFormatOption Enumeration¶
NXOpen.Annotations.CuttingPlaneSymbolBuilder.ViewNameFormatOption is an alias for NXOpen.Annotations.CuttingPlaneSymbolBuilderViewNameFormatOption
-
class
NXOpen.Annotations.
CuttingPlaneSymbolBuilderViewNameFormatOption
¶ Bases:
object
Represents whether the view name is derived from the PMI cutting plane symbol text.
Enum Members
- and A is the Text of the PMI Cutting Plane Symbol. “
- “AA”, ” View Name is in the ‘Section Prefix A-A’ format, Where Where Section Prefix is taken from PMI Preferences
and A is the Text of the PMI Cutting Plane Symbol. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.