CuttingPlaneSymbolBuilderTextPlaneRelativeArrow Enumeration¶
NXOpen.Annotations.CuttingPlaneSymbolBuilder.TextPlaneRelativeArrow is an alias for NXOpen.Annotations.CuttingPlaneSymbolBuilderTextPlaneRelativeArrow
-
class
NXOpen.Annotations.
CuttingPlaneSymbolBuilderTextPlaneRelativeArrow
¶ Bases:
object
Represents position of the text relative to the arrow option
Enum Members
Enum Member Enum Member Description Parallel The Plane of the PMI Cutting Plane Symbol Text is Parallel to its Arrow.Perpendicular The Plane of the PMI Cutting Plane Symbol Text is Perpendicular to its Arrow.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-