Constants Enumeration¶
-
class
NXOpen.Annotations.
Constants
¶ Bases:
object
Constants for annotations Enum Members
Enum Member Enum Member Description MaxLeaders The maximum number of leaders that an annotation can haveMaxLeaderIntermediatePoints The maximum number of intermediate points that a leader can have-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-