CommonWorkflowBuilder Class¶
-
class
NXOpen.Annotations.
CommonWorkflowBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.CommonWorkflowBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
DynamicAlignmentInGlobalSelection | Returns or sets the dynamic alignment in global selection determines whether drafting annotations and dimensions will automatically align or not when moving them in Global Selection. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DynamicAlignmentInGlobalSelection¶
-
CommonWorkflowBuilder.
DynamicAlignmentInGlobalSelection
¶ Returns or sets the dynamic alignment in global selection determines whether drafting annotations and dimensions will automatically align or not when moving them in Global Selection.
-------------------------------------
Getter Method
Signature
DynamicAlignmentInGlobalSelection()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DynamicAlignmentInGlobalSelection(dynamicAlignmentInGlobalSelection)
Parameters: dynamicAlignmentInGlobalSelection (bool) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
CommonWorkflowBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.