CalloutGroupBuilder Class¶
-
class
NXOpen.Annotations.
CalloutGroupBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Annotations.CalloutGroupBuilder
To create a new instance of this class, use
NXOpen.Annotations.IdSymbolCollection.CreateCalloutGroupBuilder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
CalloutModeType | Returns or sets the mode |
LayoutType | Returns or sets the layout type |
SelectCallout | Returns the selected callout |
Tag | Returns the Tag for this object. |
VerticalLeaderAttachment | Returns or sets the leader attachment to vertical callout groups |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetGroupSymbols | Gets the symbols which are grouped @return |
GetObject | Returns the object currently being edited by this builder. |
SetGroupSymbols | Groups or UnGroups the symbols based on NXOpen.Annotations.CalloutGroupBuilderMode . |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CalloutGroupBuilderLayout Enumeration | Represents group layout |
CalloutGroupBuilderMode Enumeration | Represents Group or Ungroup mode. |
CalloutGroupBuilderVerticalGroupLeaderAttachment Enumeration | Represents leader attachment for vertical callout groups. |
Property Detail¶
CalloutModeType¶
-
CalloutGroupBuilder.
CalloutModeType
¶ Returns or sets the mode
-------------------------------------
Getter Method
Signature
CalloutModeType()
Returns: Return type: NXOpen.Annotations.CalloutGroupBuilderMode
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CalloutModeType(mode)
Parameters: mode ( NXOpen.Annotations.CalloutGroupBuilderMode
) –New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
LayoutType¶
-
CalloutGroupBuilder.
LayoutType
¶ Returns or sets the layout type
-------------------------------------
Getter Method
Signature
LayoutType()
Returns: Return type: NXOpen.Annotations.CalloutGroupBuilderLayout
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LayoutType(layout)
Parameters: layout ( NXOpen.Annotations.CalloutGroupBuilderLayout
) –New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
SelectCallout¶
-
CalloutGroupBuilder.
SelectCallout
¶ Returns the selected callout
-------------------------------------
Getter Method
Signature
SelectCallout()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX7.5.0.
License requirements: None.
VerticalLeaderAttachment¶
-
CalloutGroupBuilder.
VerticalLeaderAttachment
¶ Returns or sets the leader attachment to vertical callout groups
-------------------------------------
Getter Method
Signature
VerticalLeaderAttachment()
Returns: Return type: NXOpen.Annotations.CalloutGroupBuilderVerticalGroupLeaderAttachment
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VerticalLeaderAttachment(position)
Parameters: position ( NXOpen.Annotations.CalloutGroupBuilderVerticalGroupLeaderAttachment
) –New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
GetGroupSymbols¶
-
CalloutGroupBuilder.
GetGroupSymbols
¶ Gets the symbols which are grouped
Signature
GetGroupSymbols()
Returns: Return type: list of NXOpen.Annotations.IdSymbol
New in version NX7.5.0.
License requirements: None.
SetGroupSymbols¶
-
CalloutGroupBuilder.
SetGroupSymbols
¶ Groups or UnGroups the symbols based on
NXOpen.Annotations.CalloutGroupBuilderMode
.Signature
SetGroupSymbols(symbols)
Parameters: symbols (list of NXOpen.Annotations.IdSymbol
) –New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
Validate¶
-
CalloutGroupBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.