BendTableSettingsBuilder Class¶
-
class
NXOpen.Annotations.
BendTableSettingsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.BendTableSettingsBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AutomaticUpdate | Returns or sets the automatic update option |
SortColumn | Returns or sets the column that is used to sort the bend table |
SortOnUpdate | Returns or sets the sort on update option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetColumnOrder | Returns the order of the columns in the bend table @return |
SetColumnOrder | Sets the order of the columns in the bend table |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BendTableSettingsBuilderColumnType Enumeration | This enum represents the type of the column in the bend table |
Property Detail¶
AutomaticUpdate¶
-
BendTableSettingsBuilder.
AutomaticUpdate
¶ Returns or sets the automatic update option
-------------------------------------
Getter Method
Signature
AutomaticUpdate()
Returns: Return type: bool New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
-------------------------------------
Setter Method
Signature
AutomaticUpdate(automaticUpdate)
Parameters: automaticUpdate (bool) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
SortColumn¶
-
BendTableSettingsBuilder.
SortColumn
¶ Returns or sets the column that is used to sort the bend table
-------------------------------------
Getter Method
Signature
SortColumn()
Returns: Return type: NXOpen.Annotations.BendTableSettingsBuilderColumnType
New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
-------------------------------------
Setter Method
Signature
SortColumn(sortColumn)
Parameters: sortColumn ( NXOpen.Annotations.BendTableSettingsBuilderColumnType
) –New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
SortOnUpdate¶
-
BendTableSettingsBuilder.
SortOnUpdate
¶ Returns or sets the sort on update option
-------------------------------------
Getter Method
Signature
SortOnUpdate()
Returns: Return type: bool New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
-------------------------------------
Setter Method
Signature
SortOnUpdate(sortOnUpdate)
Parameters: sortOnUpdate (bool) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
GetColumnOrder¶
-
BendTableSettingsBuilder.
GetColumnOrder
¶ Returns the order of the columns in the bend table
Signature
GetColumnOrder()
Returns: Return type: list of NXOpen.Annotations.BendTableSettingsBuilderColumnType
New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
SetColumnOrder¶
-
BendTableSettingsBuilder.
SetColumnOrder
¶ Sets the order of the columns in the bend table
Signature
SetColumnOrder(columnOrder)
Parameters: columnOrder (list of NXOpen.Annotations.BendTableSettingsBuilderColumnType
) –New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
Validate¶
-
BendTableSettingsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.