BendTableBuilder Class¶
-
class
NXOpen.Annotations.
BendTableBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Annotations.BendTableBuilder
.To create a new instance of this class, use
NXOpen.Annotations.BendTableCollection.CreateBendTableBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AnnotationOrigin | Returns the bend table origin. |
FlatPatternView | Returns the flat pattern view the bend table is associated to. |
Style | Returns the bend table style |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AnnotationOrigin¶
-
BendTableBuilder.
AnnotationOrigin
¶ Returns the bend table origin.
-------------------------------------
Getter Method
Signature
AnnotationOrigin()
Returns: Return type: NXOpen.Annotations.OriginBuilder
New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
FlatPatternView¶
-
BendTableBuilder.
FlatPatternView
¶ Returns the flat pattern view the bend table is associated to.
-------------------------------------
Getter Method
Signature
FlatPatternView()
Returns: Return type: NXOpen.Drawings.SelectDraftingView
New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
Style¶
-
BendTableBuilder.
Style
¶ Returns the bend table style
-------------------------------------
Getter Method
Signature
Style()
Returns: Return type: NXOpen.Annotations.TableStyleBuilder
New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
BendTableBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.