BaseCustomSymbolBuilderAnnotationPreferences Enumeration¶
NXOpen.Annotations.BaseCustomSymbolBuilder.AnnotationPreferences is an alias for NXOpen.Annotations.BaseCustomSymbolBuilderAnnotationPreferences
-
class
NXOpen.Annotations.
BaseCustomSymbolBuilderAnnotationPreferences
¶ Bases:
object
Enum for Annotation Preferences This is used by
NXOpen.Annotations.BaseCustomSymbolBuilder.AnnotationPreferences
andNXOpen.Annotations.BaseCustomSymbolBuilder.AnnotationPreferences
to set the annotation preferences for a symbolEnum Members
.
- . csv-table::
header: “Enum Member”, “Enum Member Description” “UseCurrent”, ” Current preferences ” “UseDefinition”, ” Defined preferences “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.