AssociativeTextPropertyType Enumeration¶
NXOpen.Annotations.AssociativeText.PropertyType is an alias for NXOpen.Annotations.AssociativeTextPropertyType
-
class
NXOpen.Annotations.
AssociativeTextPropertyType
¶ Bases:
object
the associative text property type to be used with the object
Enum Members
Enum Member Enum Member Description DrawingNumberOfSheets Drawing sheet number of sheetsDrawingNumberOfPrimarySheets Drawing sheet number of primary sheetsDrawingSheetName Drawing sheet nameDrawingSheetNumber Drawing sheet numberDrawingSheetRevision Drawing sheet revisionDrawingSheetScaleNumerator Drawing sheet scale numeratorDrawingSheetScaleDenominator Drawing sheet scale denominatorDrawingSheetSize Drawing sheet sizeDrawingSheetUnits Drawing sheet unitsDrawingSheetZone Drawing sheet zoneDrawingSheetProjectionAngle Drawing sheet projection angleDrawingMasterPartName Drawing master part nameDrawingPartName Drawing part nameDrawingViewPrefix Drawing view prefixDrawingViewRotationAngle View rotation angle-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-