ArbitraryTargetData Class¶
-
class
NXOpen.Annotations.
ArbitraryTargetData
¶ Bases:
NXOpen.Annotations.DatumTargetData
Represents arbitrary datum target data
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
DatumLabel | Returns or sets the datum label. |
Index | Returns or sets the target index. |
UpperText | Returns or sets the upper text. |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetSimpleDraftingAidPreferences | Returns the SimpleDraftingAidPreferences object @return Datum target preferences |
SetSimpleDraftingAidPreferences | Sets the SimpleDraftingAidPreferences object |
Property Detail¶
UpperText¶
-
ArbitraryTargetData.
UpperText
¶ Returns or sets the upper text.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
-------------------------------------
Getter Method
Signature
UpperText()
Returns: Upper text Return type: str New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpperText(upperText)
Parameters: upperText (str) – New upper text New in version NX4.0.0.
License requirements: None.