AppendedTextEditorBuilder Class¶
-
class
NXOpen.Annotations.
AppendedTextEditorBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Annotations.AppendedTextEditorBuilder
builderTo create a new instance of this class, use
NXOpen.Annotations.DimensionCollection.CreateAppendedTextEditorBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AppendedTextBuilder | Returns the appended text builder |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetDimensions | Sets all the dimensions to the builder |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AppendedTextBuilder¶
-
AppendedTextEditorBuilder.
AppendedTextBuilder
¶ Returns the appended text builder
-------------------------------------
Getter Method
Signature
AppendedTextBuilder()
Returns: Return type: NXOpen.Annotations.AppendedTextBuilder
New in version NX9.0.0.
License requirements: None.
Method Detail¶
SetDimensions¶
-
AppendedTextEditorBuilder.
SetDimensions
¶ Sets all the dimensions to the builder
Signature
SetDimensions(dimensions)
Parameters: dimensions (list of NXOpen.Annotations.Dimension
) – Dimensions ArrayNew in version NX9.0.0.
License requirements: None.
Validate¶
-
AppendedTextEditorBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.